Hardware requirements
Micro USB cable
MIMX8ULP-EVK/EVK9 board
J-Link Debug Probe
5V power supply
Personal Computer
Board settings
No special settings are required.
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Build the project and generate the flash.bin file of single boot. Refer to the ‘Getting Started with MCUXpresso SDK for EVK-MIMX8ULP.pdf’.
Connect a type-c USB cable between the host PC and the USB0 port on the target board.
Connect 5V power supply to the board.
Download flash.bin into emmc with uuu. Refer to ‘Getting Started with MCUXpresso SDK for EVK-MIMX8ULP.pdf’
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Switch the SW1 to re-power the board.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
High Byte test success
----- Refresh test start -----
----- None-window mode -----
Refresh wdog32 0 time
Refresh wdog32 1 time
Refresh wdog32 2 time
Refresh wdog32 3 time
Refresh wdog32 4 time
Refresh wdog32 5 time
Refresh wdog32 6 time
Refresh wdog32 7 time
Refresh wdog32 8 time
Refresh wdog32 9 time
----- Window mode -----
Refresh wdog32 0 time
Refresh wdog32 1 time
Refresh wdog32 2 time
----- Refresh test success  -----
----- End of WDOG32 example  -----