Hardware requirements
- Mini/micro USB cable 
- EVK-MIMXRT1020 board 
- Personal Computer 
- SD card 
Board settings
Please insert the SDCARD into card slot(J15), make sure C28 is welded. Note: If you want to use a SD3.0 card with SD3.0 protocol, just insert a SD3.0 card into the card slot will be ok.
Prepare the Demo
- Connect a micro USB cable between the PC host and the OpenSDA USB port on the board. 
- Open a serial terminal on PC for OpenSDA serial device with these settings: - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Insert SD card to card slot 
- Download the program to the target board. 
- Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. 
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
Card size xxxxx bytes
Working condition:
  Voltage : xxxV
  Timing mode: xxx
  Freq : xxx HZ
Read/Write/Erase the card continuously until encounter error......
Write/read one data block......
Compare the read/write content......
The read/write content is consistent.
Write/read multiple data blocks......
Compare the read/write content......
The read/write content is consistent.
Erase multiple data blocks......
Input 'q' to quit read/write/erase process.
Input other char to read/write/erase data blocks again.
Note: To debug in qspiflash, following steps are needed:
- Select the flash target and compile. 
- Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23. 
- Start debugging in IDE. - Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.