Hardware requirements
Mini/micro USB cable
MIMXRT1040-EVK board
Personal Computer
Board settings
Remove jumper J80.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
CMP polling Example
Then change CMP analog input, and watch the change of LED. - CMP1_IN1 (J17-9) connected to VCC =3.3V (J32-4): USER LED on - CMP1_IN1 (J17-9) connected to GND (J32-6): USER LED off