Hardware requirements
Mini/micro USB cable
MIMXRT1040-EVK board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
Press anykey to start the example...
EWM example
Press SW8 to expire EWM
EWM interrupt is occurred
Press SW8 to expire EWM again
Note: This case will run to HardFault_Handler on IAR flexspi_nor_debug/flexspi_nor_release target. This issue will be fixed in later release.