Hardware requirements

  • Micro USB cable

  • MIMXRT1040-EVK board

  • RK043FN02H-CT or RK043FN66HS-CT6 LCD board

  • Personal Computer

Board settings

  1. Connect the RK043FN02H-CT or RK043FN66HS-CT6 to board.

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Build the project, the project uses RK043FN66HS-CT6 by default, to use other panels, set the coresponding panel to y in prj.conf under board example folder before project generation. The supported panels can be found in examples_boards<board>\project_segments\display_support\Kconfig.prjseg. Or change the macro DEMO_PANEL in mcux_config.h of the project, which number represents which panel can be found in display_support.h and mcux_config.h

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. Running the demo =============== When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

PXP Rotate example start...