MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • EVK-MIMXRT1064 board

  • JLink Plus

  • 5V power supply

  • Personal Computer

  • RK043FN02H-CT or RK043FN66HS-CT6 LCD board (RK043FN02H-CT and RK043FN66HS-CT6 are compatible)

  • SD card

Board settings#

  1. Connect the RK043FN02H-CT or RK043FN66HS-CT6 to board.

  2. Prepare the H264 files and save in SD card.

  3. Insert the SDCARD into card slot.

Prepare the Demo#

The demo use RK043FN66HS-CT6 panel by default, to use other panel, set the coresponding panel DEMO_PANEL_xxx(without ‘_SUPPORT’) to y in prj.conf under board example folder before project generation. The supported panels can be found in examples_boards<board>\project_segments\display_support\Kconfig.prjseg. Or change the macro DEMO_PANEL in mcux_config.h of the project, which number represents which panel can be found in display_support.h and mcux_config.h

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo#

If this example runs correctly, pictures are shown in the lcd panel.