MCUXpresso SDK Documentation

Hardware requirements#

  • Mini/micro USB cable

  • EVK-MIMXRT1064 board

  • Personal Computer

Board settings#

MCUBoot layout#

Region

From

To

Size

MCUboot code

0x70000000

0x7003FFFF

256kB

Primary slot

0x70040000

0x7013FFFF

1024kB

Secondary slot

0x70140000

0x7023FFFF

1024kB

  • MCUBoot header size is set to 1024 bytes

  • Signing algorithm is ECDSA-P256

  • Write alignment is 4 bytes

  • MCUBoot is configured to use its DIRECT_XIP image handling strategy

  • Flash remapping HW feature is used for zero-overhead image swapping

  • To manually enter serial recovery mode, keep the user button pressed during reset, then release it

Image signing example#

imgtool sign   --key sign-ecdsa-p256-priv.pem
               --align 4
               --version 1.1
               --slot-size 0x100000
               --header-size 0x400
               --pad-header
               ota_mcuboot_basic.bin
               ota_mcuboot_basic.SIGNED.bin

Note that for the first image flashed manually together with the bootloader additional imgtool options “–pad” and “–confirm” must be used. Otherwise the bootloader would reject the image for missing data in the trailer area.

Custom configuration - Encrypted XIP#

Region

From

To

Size

MCUboot code

0x70000000

0x7003FFFF

256kB

Primary slot

0x70040000

0x7013FFFF

1024kB

Secondary slot

0x70140000

0x7023FFFF

1024kB

Encryption metadata

0x70240000

0x70240FFF

4kB

This custom build generates a project with predefined configuration to utilize Encrypted XIP mode. For more information please see Encrypted XIP and MCUboot.

  • MCUBoot header size is set to 1024 bytes

  • Signing algorithm is ECDSA-P256

  • Write alignment is 4 bytes

  • MCUBoot is configured for Encrypted XIP mode using modified MCUBOOT_OVERWRITE_ONLY image update strategy

  • MCUboot uses ECDH-P256 to secure AES key for image encryption

  • Primary slot is encrypted by BEE module to utilize encrypted XIP

Image signing example:

imgtool sign --key sign-ecdsa-p256-priv.pem
             --align 4
             --version 1.1
             --slot-size 0x200000
             --header-size 0x400
             --max-sectors 59
             --pad-header
             -E enc-ec256-pub.pem
             ota_mcuboot_basic.bin
             ota_mcuboot_basic.SIGNED.bin

Project building example:

The project is built using west tool. For more information please see MCUXpresso SDK documentation.

Bootloader:

west build -p always examples/ota_examples/mcuboot_opensource --toolchain iar --config flexspi_nor_debug -b evkmimxrt1064 -t guiproject -DCONF_FILE="examples/ota_examples/_custom_cfg/rt1064/mcuboot_opensource.conf" -d builds/mcuboot

OTA application:

west build -p always examples/ota_examples/ota_mcuboot_basic --toolchain iar --config flexspi_nor_debug -b evkmimxrt1064 -t guiproject -DCONF_FILE="examples/ota_examples/_custom_cfg/rt1064/ota_mcuboot_basic.conf" -d builds/ota_mcuboot_basic