Hardware requirements#
Micro USB cable
MIMXRT1160-EVK board
JLink Plus
5V power supply
Personal Computer
RK055MHD091 panel or RK055AHD091 panel or RK055IQH091 panel
SD card
Board settings#
Connect the RK055MHD091-CTG LCD board to J48.
Unzip the pics.zip, place the png pictures to the SD card.
Please make sure R136 is weld for GPIO card detect and then insert the SDCARD into card slot(J15).
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Build the project, the project uses RK055MHD091 by default, to use other panels, set the coresponding panel DEMO_PANEL_xxx(without ‘_SUPPORT’) to y in prj.conf under board example folder before project generation. The supported panels can be found in examples_boards<board>\project_segments\display_support\Kconfig.prjseg. Or change the macro DEMO_PANEL in mcux_config.h of the project, which number represents which panel can be found in display_support.h and mcux_config.h
Insert SD card to card slot
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
If this example runs correctly, pictures are shown in the lcd panel one by one.