Hardware requirements#
Mini/micro USB cable
MIMXRT1160-EVK board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo#
When the demo runs successfully, the following message is displayed in the terminal:
*********QUADTIMER EXAMPLE START*********
****Timer use-case, 50 millisecond tick.****
Timer interrupt has occured !
Timer interrupt has occured !
Timer interrupt has occured !
Timer interrupt has occured !
Timer interrupt has occured !
Timer interrupt has occured !
Timer interrupt has occured !
Timer interrupt has occured !
Timer interrupt has occured !
Timer interrupt has occured !
****Chain Timer use-case, 10 second tick.****
Timer interrupt has occured !
Timer interrupt has occured !
Timer interrupt has occured !
Timer interrupt has occured !
Timer interrupt has occured !
*********QUADTIMER EXAMPLE END.*********
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~