Hardware requirements
- Mini/micro USB cable 
- MIMXRT1180-EVK board 
- Personal Computer 
- Headphone(OMTP standard) 
Board settings
No special settings are required.
Prepare the Demo
- Connect a USB cable between the host PC and the OpenSDA USB port on the target board. 
- Open a serial terminal with the following settings: - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board. 
- Insert the headphones into the headphone jack on MIMXRT1180-EVK board (J101). 
- Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. 
Running the demo
When the demo runs successfully, you can hear the tone and the log would be seen on the OpenSDA terminal like:
SAI functional interrupt example started!
SAI functional interrupt example finished!