Hardware requirements

  • Micro USB cable

  • TFT Proto 5” CAPACITIVE board HW REV 1.01 by Mikroelektronika. (Named as SSD1963 panel in project. Not necessary if use MIPI panel)

  • EVK-MIMXRT595

  • Personal Computer

  • RK055AHD091 MIPI panel (Not necessary if use other panel)

  • RK055MHD091 MIPI panel (Not necessary if use other panel)

  • RM67162(G1120B0MIPI) smart MIPI panel (Not necessary if use other panel)

  • CO5300(ZC143AC72MIPI) smart MIPI panel (Not necessary if use other panel)

  • SD card

Board settings

  1. To use SSD1963 panel: Connect SSD1963 panel to J43.

  2. Make sure resistors R691~R697 are populated and resistors R611~R620,R660, R661 are removed.

  3. To use MIPI panel: Connect MIPI panel to J44.

  4. Unzip the pics.zip, place the jpg pictures to the SD card.

  5. Insert the SDCARD into card slot.

Prepare the Demo

The demo use RK055MHD091 MIPI panel by default, to use other panel, set the coresponding panel DEMO_PANEL_xxx(without ‘_SUPPORT’) to y in prj.conf under board example folder before project generation. The supported panels can be found in examples_boards<board>\project_segments\display_support\Kconfig.prjseg. Or change the macro DEMO_PANEL in mcux_config.h of the project, which number represents which panel can be found in display_support.h and mcux_config.h

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

When Package is used

Modify DEMO_PANEL in mcux_config.h. #define DEMO_PANEL 4 for “MikroE TFT Proto 5” CAPACITIVE FlexIO panel. #define DEMO_PANEL 0 for “RK055HDMIPI4M” MIPI Rectangular panel. #define DEMO_PANEL 3 for “G1120B0MIPI” MIPI Circular panel. #define DEMO_PANEL 2 for “RK055MHD091A0-CTG MIPI Rectangular panel.(default)

Running the demo

If this example runs correctly, pictures are shown in the lcd panel one by one.