Hardware requirements
Micro USB cable
EVK-MIMXRT685 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows example output of the frequency measure demo in the terminal window:
Capture source: External clock (clk_in) (main system clock reference), reference frequency = 250105263 Hz
Computed frequency value = 23999301 Hz
Expected frequency value = 24000000 Hz
Capture source: RTC32K oscillator (main clock reference), reference frequency = 250105263 Hz
Computed frequency value = 5001265 Hz
Expected frequency value = 5002105 Hz
Capture source: FRO oscillator (main clock reference), reference frequency = 48000000 Hz
Computed frequency value = 52240185 Hz
Expected frequency value = 48000000 Hz