Hardware requirements#
Micro USB cable
FRDM-IMX937 board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings#
No special settings are required.
Please note this application can’t support running with Linux BSP!
Prepare the Demo#
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo#
When the demo runs successfully, will get the similar messages on the terminal.
Timestamp1 = 01c98d6
Test the delay function, delay for 1 second
Start time = 01cb123
End time = 02bfbd3