Hardware requirements#
Micro USB cable
FRDM-IMX937 board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board
Connect a USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.