Hardware requirements#
Type-C USB cable
FRDM-IMX952 board
J-Link Debug Probe
15V~20V USB Type-C PD power supply
Personal Computer
Board settings#
Connect J18-3 (GPIO_IO02, FLEXIO1_FLEXIO[2]) and J18-4 (GND) to oscilloscope
Please note this application can’t support running with Linux BSP!#
Note#
Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.
Prepare the Demo#
Connect 15V~20V USB Type-C PD power supply and J-Link Debug Probe to the board, switch SW1 to power on the board.
Connect a Type-C USB cable between the host PC and the J1 USB Type-C port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo#
When the example runs successfully, if the input duty cycle range is 0~100, You can see similar information from the terminal as follows and square wave observed by oscilloscope will modify duty cycle due to input:
FLEXIO_PWM demo start.
Please input a value (0 - 100) to set duty cycle: 10
Input value is 10
PWM duty cycle is: 10
PWM leave is: 0
Please input a value (0 - 100) to set duty cycle: 150
Input value is 150
Your value is output of range.
Set pwm output to IDLE.
Please input pwm idle status (0 or 1): 1
Input IDLE state value is 1
PWM leave is: 1
Please input a value (0 - 100) to set duty cycle:
......
Note:
The duty cycle of the PWM is variable, except for the idle state, 0 and 100.
If the input duty cycle range exceeds 100, the pwm will be set to idle state
If the set pwm idle value is out of range, it will output “Your value is output of range.” and then return to set the duty cycle.