Hardware requirements#
Mini/micro USB cable
FRDM-IMXRT1186 board
Personal Computer
An encoder with PHASE A/B signals.
Board settings#
Change Jumper J30 and J35 from 1-2 to 2-3
For pin connection between board and encoder, J1.14 -> kXBAR1_InputRESERVED18 -> kXBAR1_OutputEnc1Phasea -> EQDC_PHA J51.10 -> kXBAR1_InputRESERVED19 -> kXBAR1_OutputEnc1Phaseb -> EQDC_PHB J3.21 -> kXBAR1_InputRESERVED23 -> kXBAR1_OutputEnc1Index -> EQDC_INDEX
Prepare the Demo#
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Connect the wires between encoder and the MCU board. See to the code for pin mux setting in function “BOARD_InitPins()”.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.