Hardware requirements#
Type-C USB cable
FRDM-IMXRT700 board
Personal Computer
SD Card
Board settings#
Recommend SD Cards used to run the example
Brand |
Mode |
Size |
Speed Class |
Video Speed Class |
UHS |
A1 |
A2 |
|---|---|---|---|---|---|---|---|
SanDisk |
Ultra |
16GB |
10 |
- |
- |
YES |
- |
SanDisk |
Extreme |
64GB |
- |
V30 |
3 |
- |
YES |
SanDisk |
Ultra Plus |
32GB |
10 |
V10 |
- |
YES |
- |
SanDisk |
ImageMate PRO |
32GB |
- |
V30 |
3 |
YES |
- |
Kingston |
- |
16GB |
10 |
- |
1 |
- |
- |
Prepare the Demo#
Connect a USB cable between the PC host and the Debug port on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Please insert the SDCARD into card slot(J47)
Running the demo#
When the demo runs successfully, the log would be seen on the terminal like:
FATFS example to demonstrate how to use FATFS with SD card.
Please insert a card into board.
Card inserted.
Make file system......The time may be long if the card capacity is big.
Create directory......
Create a file in that directory......
Create a directory in that directory......
List the file in that directory......
General file : F_1.DAT.
Directory file : DIR_2.
Write/read file until encounters error......
Write to above created file.
Read from above created file.
Compare the read/write content......
The read/write content is consistent.
Input 'q' to quit read/write.
Input other char to read/write file again.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~