MCUXpresso SDK Documentation

Hardware requirements#

  • Type-C USB cable

  • FRDM-IMXRT700 board

  • Personal Computer

  • SD Card

Board settings#

Recommend SD Cards used to run the example

Brand

Mode

Size

Speed Class

Video Speed Class

UHS

A1

A2

SanDisk

Ultra

16GB

10

-

-

YES

-

SanDisk

Extreme

64GB

-

V30

3

-

YES

SanDisk

Ultra Plus

32GB

10

V10

-

YES

-

SanDisk

ImageMate PRO

32GB

-

V30

3

YES

-

Kingston

-

16GB

10

-

1

-

-

Prepare the Demo#

  1. Connect a USB cable between the PC host and the Debug port on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Please insert the SDCARD into card slot(J47)

Running the demo#

When the demo runs successfully, the log would be seen on the terminal like:

SDCARD freertos example.

Card inserted.

Read/Write/Erase the card continuously until encounter error......

Write/read one data block......
Compare the read/write content......
The read/write content is consistent.
Write/read multiple data blocks......
Compare the read/write content......
The read/write content is consistent.
Erase multiple data blocks......

Input 'q' to quit card access task.
Input other char to read/write/erase data blocks again.

If sd card is not inserted before example run, then more log will generated like:

SDCARD freertos example.

Please insert a card into board.