Hardware requirements#
Type-C USB cable
FRDM-IMXRT700
Personal Computer
RaspberryPi Panel
Board settings#
To use Raspberry panel: Connect the panel to J8. Then connect the panel’s 5V pin to JP43-1, GND pin to JP43-2.
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Steps to configure the panels#
Running the demo#
When the example runs, you can see a clock with high render quality on the screen.