Hardware requirements
- Micro USB cable 
- FRDM-K32L2B board 
- Personal Computer 
Board settings
The example requires connection between the flexio output pin and LED pin.
- J2-4, J2-12 connected Use oscilloscope to measure output the 200KHz PWM signal pin at J2-4 pin of board. 
Prepare the Demo
- Connect a USB cable between the PC host and the OpenSDA USB port on the board. 
- Open a serial terminal with these settings: - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board. 
- Either press the reset button on your board or launch the debugger in your IDE to begin running the example. 
Running the demo
When the example runs successfully, if the input duty cycle range is 0~100, You can see similar information from the terminal as follows:
FLEXIO_PWM demo start.
Please input a value (0 - 100) to set duty cycle: 10
Input value is 10
PWM duty cycle is: 10
Please input a value (0 - 100) to set duty cycle: 150
Input value is 150
Your value is output of range.
Set pwm output to IDLE.
Please input pwm idle status (0 or 1): 1
Input IDLE state value is 1
Please input a value (0 - 100) to set duty cycle: 
......
Note:
- The duty cycle of the PWM is variable, except for the idle state, 0 and 100. 
- If the input duty cycle range exceeds 100, the pwm will be set to idle state 
- If the set pwm idle value is out of range, it will output “Your value is output of range.” and then return to set the duty cycle.