Hardware requirements
- Micro USB cable 
- FRDM-KE15Z board 
- Personal Computer 
Board settings
The example requires connecting between LPSPI0 pins and LPSPI1 pins The connection should be set as following: MASTER connect to SLAVE Pin Name Board Location Pin Name Board Location SOUT J3 pin 7 SIN J2 pin 10 SIN J3 pin 9 SOUT J2 pin 8 SCK J3 pin 11 SCK J2 pin 12 PCS3 J3 pin 5 PCS3 J2 pin 6
Prepare the Demo
- Connect a USB cable between the host PC and the OpenSDA USB port on the target board. 
- Open a serial terminal with the following settings: 
- 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
- Download the program to the target board. 
- Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. 
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPSPI functional interrupt example start.
This example use one lpspi instance as master and another as slave on one board.
Master uses interrupt way and slave uses interrupt way.
Note that some LPSPI instances interrupt is in INTMUX ,you should set the intmux when you porting this example accordingly
Please make sure you make the correct line connection. Basically, the connection is:
LPSPI_master -- LPSPI_slave
   CLK      --    CLK
   PCS      --    PCS
   SOUT     --    SIN
   SIN      --    SOUT
LPSPI transfer all data matched!
End of example.