MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • FRDM-KE15Z board

  • Personal Computer

Board settings#

No special settings are required.

Prepare the Demo#

  1. Connect a USB cable between the PC host and the OpenSDA USB port on the board.

  2. Download the program to the target board.

  3. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

When the demo runs successfully, you will find the LED is blinking.