Hardware requirements#
Type-C USB cable
FRDM-KW43 Board
Personal Computer
Board settings#
Prepare the Demo#
Connect a USB cable between the host PC and the FRDM board J28.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo#
The following lines are printed to the serial terminal when the demo program is executed.
Press anykey to start the example...
EWM example
Press SW3 to expire EWM
EWM interrupt is occurred
Press SW3 to expire EWM again