Hardware requirements#
Type-C USB cable
FRDM-KW43 Board
Personal Computer
Board settings#
Connect J23-8 to a voltage source.
Prepare the Demo#
Connect a USB cable between the host PC and the FRDM board J28.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The following lines are printed to the serial terminal when the demo program is executed.
LPADC DMA3 Example
ADC Full Range: XXXX
Please press any key to trigger the conversion.
ADC conversion word: 0xXXXXXXXX
ADC conversion value: XXXX