MCUXpresso SDK Documentation

Hardware requirements#

  • Type-C USB cable

  • FRDM-MCXA153 board

  • Personal Computer

Board settings#

No special settings are required.

Prepare the Demo#

  1. Connect a Type-C USB cable between the host PC and the MCU-Link port(J15) on the target board.

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

  5. The J4 pin 8 (ADC0_A0) on EVK board is used to monitor the voltage.

Running the demo#

The following lines are printed to the serial terminal when the demo program is executed.

LPADC EDMA Example
Configuring LPADC...
ADC Full Range: 4096
Configuring LPADC EDMA...
Press any key to print output buffer:

0 = 3192
1 = 3192
2 = 3184
3 = 3184