Hardware requirements

  • Type-C USB cable

  • FRDM-MCXA153 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a Type-C USB cable between the host PC and the MCU-Link port(J15) on the target board.

  2. Open a serial terminal on PC for the serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following lines are printed to the serial terminal when the demo program is executed.

Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6