Hardware requirements
Type-C USB cable
FRDM-MCXA266 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
Utick example start...
UTICK delay 1 second...
UTICK delay 1 second...