MCUXpresso SDK Documentation

Hardware requirements#

  • Type-C USB cable

  • FRDM-MCXA577 board

  • Personal Computer

Board settings#

No special settings are required.

Prepare the Demo#

  1. Connect the type-c and mini USB cable between the PC host and the USB ports on the board.

  2. Open a serial terminal on PC for the serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

The following lines are printed to the serial terminal when the demo program is executed.

Press anykey to start the example...

EWM example
Press SW3 to expire EWM
EWM interrupt is occurred
Press SW3 to expire EWM again