Hardware requirements#
Type-C USB cable
FRDM-MCXA577 board
Personal Computer
Board settings#
ADC0 CH0A input signal J8-21(P2_0).
Prepare the Demo#
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The following lines are printed to the serial terminal when the demo program is executed.
LPADC EDMA Example
Configuring LPADC...
ADC Full Range: 4096
Configuring LPADC EDMA...
Press any key to print output buffer:
0 = 3192
1 = 3192
2 = 3184
3 = 3184