Hardware requirements
Type-C USB cable
FRDM-MCXC041 board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
COP example start!
COP refresh 1 time
COP refresh 2 time
COP refresh 3 time
COP refresh 4 time
COP refresh 5 time
COP refresh 6 time
COP refresh 7 time
COP refresh 8 time
COP refresh 9 time
COP refresh 10 time
COP will timeout and chip will be reset
Reset due to COP timeout
COP example ends!