Hardware requirements#
Type-C USB cable
FRDM-MCXL255 board
Personal Computer
Board settings#
Provide 0-3.3V voltage to J6-1 “AN” pin (ADC ch0 P3_9).
Prepare the Demo#
Connect a USB Type-C cable between the host PC and the MCU-Link USB port (J16) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The following lines are printed to the serial terminal when the demo program is executed.
LPADC Polling Example
ADC Full Range: 65536
Please press any key to get user channel's ADC value.
ADC value: 35596