MCUXpresso SDK Documentation

Hardware requirements#

  • Type-C USB cable

  • FRDM-MCXN236 board

  • Personal Computer

  • Headphone(OMTP standard)

Board settings#

No special settings are required.

Prepare the Demo#

  1. Connect a USB cable between the PC host and the MCU-Link USB port on the board.

  2. Open a serial terminal with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Insert the headphones into the headphone jack on board (J14).

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

Note: This demo outputs 1000HZ sine wave audio signal. When the demo runs successfully, you can hear the tone and the log would be seen on the MCU-Link terminal like:

 SAI functional interrupt example started!



 SAI functional interrupt example finished!