Hardware requirements#
Type-C USB cable
FRDM-MCXN947 board
Personal Computer
Board settings#
Prepare the Demo#
Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the example runs successfully, you can see the similar information from the terminal as below.
ITRC Peripheral Driver Example
Pass: No Event/Action triggered in STATUS after Init
Enable ITRC IRQ Action response to SW Event 0
Trigger SW Event 0
ITRC IRQ Reached! ITRC STATUS: Input event IN14 occured!
Clear ITRC IRQ and SW Event 0 STATUS
Disable ITRC IRQ Action response to SW Event 0
Trigger SW Event 0
Pass: No Action triggered
End of example