Hardware requirements
- Type-C USB cable 
- FRDM-MCXW71 Board 
- Personal Computer 
Board settings
Prepare the Demo
- Connect a USB cable between the host PC and UART0 on the target board. 
- Open a serial terminal with the following settings: - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board. 
- Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. 
Running the demo
Copyright 2024 NXP
LOG SHELL>>