Hardware requirements#
Type-C USB cable
FRDM-MCXW71 Board
Personal Computer
Board settings#
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo#
Connect a USB cable between the host PC and the FRDM board J10.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the demo runs successfully, you will detect voltage toggle on J4.P31 of the EBB MB board. If the EVK board is used then the green led will blink.