Hardware requirements
Type-C USB cable
FRDM-MCXW71 Board
Personal Computer
Board settings
This Example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
PFlash Example Start
PFlash Information:
Program Flash block bass address: 0, Hex: (0x0)
Program Flash block Size: 1024 KB, Hex: (0x100000)
Program Flash block Sector Size: 8 KB, Hex: (0x2000)
Program Flash block count Size: 1
Total Program Flash Size: 1024 KB, Hex: (0x100000)
Erase a sector of flash
Successfully Erased Sector 0xfe000 -> 0x100000
Program a buffer to a phrase of flash
Successfully Programmed and Verified Location 0xfe000 -> 0xfe010
End of PFlash Example
~~~~~~~~~~~~~~~~~~~~~~~
And you will find the flash hase been programed.