Hardware requirements#
Type-C USB cable
FRDM-MCXW72 Board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The following lines are printed to the serial terminal when the demo program is executed.
Status=DD000001, Reply=AA000002
F32 2x1 x 1x3 MAT MULT Test Passed: Status=DD000002, Reply=AA000003
F32 2x2 MAT MULT Test Passed: Status=DD000003, Reply=AA000004
CF32 2x1 x 1x3 MAT MULT Test Passed: Status=DD000004, Reply=AA000005
CF32 2x2 MAT MULT Test Passed: Status=DD000005, Reply=AA000006
F32 MAT MULT Test Passed: Status=DD000006, Reply=AA000007
CF32 MAT MULT Test Passed: Status=DD000007, Reply=AA000008