MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • FRDM-RW612 board

  • Personal Computer

Board settings#

No special settings are required.

Prepare the Demo#

  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J10) on the board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the example.

Running the demo#

The log below shows the output of the demo in the terminal window:

 Temperature measurement example.
 Please press any key to get the temperature.
 Current temperature is: 24.379 degrees Celsius.
 Current temperature is: 24.859 degrees Celsius.
 Current temperature is: 24.859 degrees Celsius.
 Current temperature is: 24.859 degrees Celsius.
 Current temperature is: 24.859 degrees Celsius.