Hardware requirements
Micro USB cable
IMX95LPD5-EVK board
12V~20V power supply
Personal Computer
Board settings
This example uses NETC ENETC2 10G port.
Prepare the Demo
Connect 12V~20V power supply to the board.
Connect a micro USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Program the Linux BSP to SD/eMMC. Then program flash.bin of this demo.
Switch SW4 to power on the board.
Note: the flash.bin is flash_all target with mx95netc.cfg System Manager image. For A core Linux BSP side usage, refer to Linux BSP User Guide “11.6.1 i.MX95 ENETC share use case”.
Running the demo
When the demo runs, the log would be seen on the terminal like below. Both A core Linux BSP and M core share NETC ENETC2 10G port to use.
Initializing PHY...
[LINK STATE] netif=0, state=up, speed=1000M_full
************************************************
 DHCP example
************************************************
 DHCP state       : SELECTING
 DHCP state       : REQUESTING
 DHCP state       : CHECKING
 DHCP state       : BOUND
 IPv4 Address     : 192.168.0.4
 IPv4 Subnet mask : 255.255.255.0
 IPv4 Gateway     : 192.168.0.1