Hardware requirements
- Micro USB cable 
- Personal Computer 
- KW45B41Z-EVK board 
Board settings
No special settings are required.
Prepare the Demo
- Connect the micro and mini USB cable between the PC host and the USB ports on the board. 
- Open a serial terminal on PC for the serial device with these settings: - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board. 
- Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.