MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • Personal Computer

  • KW47-EVK board

Board settings#

No special settings are required.

Prepare the Demo#

  1. Connect a USB cable between the host PC and the EVK board J14.

  2. Open a serial terminal on PC for the serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

The following lines are printed to the serial terminal when the demo program is executed.

"ABCD | EFGH"
"1234 | 5678"
"ABCD | EFGH"
"1234 | 5678"