MCUXpresso SDK Documentation

Hardware requirements#

  • KW47-EVK Board

  • USB-C cable

  • Personal Computer

Board settings#

MCUBoot layout#

Region

From

To

Size

MCUboot code

0x00000000

0x0003FFFF

256kB

Primary slot

0x00040000

0x0011FFFF

896kB

Secondary slot

0x00120000

0x001FFFFF

896kB

  • MCUBoot header size is set to 512 bytes

  • Signing algorithm is ECDSA-P256

  • Write alignment is 16 bytes

  • Uses image swapping by SWAP_USING_MOVE

  • To manually enter serial recovery mode, keep the SW2 button pressed during reset, then release it

Image signing example#

imgtool sign --key sign-ecdsa-p256-priv.pem
             --align 16
             --version 1.1
             --slot-size 0xE0000
             --header-size 0x400
             --max-sectors 111
             --pad-header
             -E enc-ec256-pub.pem
             ota_mcuboot_basic.bin
             ota_mcuboot_basic.SIGNED.bin