Hardware requirements#
Micro USB cable
LPCXpresso51U68 board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J6) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Running the demo#
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
The following lines are printed to the serial terminal when the demo program is executed.
Group GPIO input interrupt example
GINT0 and GINT1 events are configured
Press corresponding switches to generate events
This example configures “Group GPIO interrupt 0”” to be invoked when SW1 switch is pressed by the user. The interrupt callback prints “GINT0 event detected” message on the serial terminal. “”Group GPIO interrupt 1”” is configured to be invoked when both the switches SW2 and SW3 are pressed at the same time. The interrupt callback prints “GINT1 event detected” message on the serial terminal.