Hardware requirements
Micro USB cable
LPCXpresso55S06 board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the LPC-Link USB port (J1) on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
Usart functional interrupt example
Board receives characters then sends them out
Now please input: