Hardware requirements#
Mini/micro USB cable
LPCXpresso55S16 board
Personal Computer
Board settings#
The jumper setting: Default jumpers configuration does not work, you will need to add JP20 and JP21 (JP22 optional for ADC use)
Prepare the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the example runs successfully, the following message is displayed in the terminal:
Flash driver API tree Demo Application...
Initializing flash driver...
Flash init successfull!!. Halting...
PFlash Example Start
kFLASH_PropertyPflashBlockBaseAddr = 0x0
kFLASH_PropertyPflashSectorSize = 32768
kFLASH_PropertyPflashTotalSize = 655360
kFLASH_PropertyPflashPageSize = 0x200
Calling FLASH_Erase() API...
Done.
Done!
Calling FLASH_VerifyErase() API...
Done.
FLASH Verify Erase successful!
Calling FLASH_Program() API...
Done.
Calling FLASH_VerifyProgram() API...
Done.
FLASH Verify Program successful!
Successfully Programmed and Verified Location 0x80000 -> 0x80200
Done!