Hardware requirements#
Micro USB cable
Personal Computer
LPCXpresso55S36 board
Board settings#
This example project uses HSCMP to compare the voltage signal input from channel 3(P1_5) with the voltage signal(half of VREF_OUT) output by HSCMP’s internal DAC and output different result. LED_RED will turn ON/OFF corresponding to different result. So the voltage signal input from P1_28 should be changed to observe the dynamical LED state.
Input signal to J9-9
Prepare the Demo#
Connect the micro and mini USB cable between the PC host and the USB ports(J1) on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The following lines are printed to the serial terminal when the demo program is executed.
HSCMP polling Example.