Hardware requirements
- Mini/micro USB cable 
- LPCXpresso802 board 
- Personal Computer 
Board settings
No special settings are required.
Prepare the Demo
- Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board 
- Open a serial terminal with the following settings: - 9600 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board. 
- Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. 
Running the demo
The log below shows the output of the hello world demo in the terminal window:
Usart polling example.
Board will send back received characters.
Now, please input any character: