Toolchain Supported#
IAR embedded Workbench 8.50.5
Keil MDK 5.31
GCC ARM Embedded 9.2.1
MCUXpresso 11.2.0
Hardware Requirements#
Mini/micro USB cable
LPCXpresso845MAX board
Personal Computer
Board Settings#
No special settings are required.
Run the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP port(J4 on the board).
Choose an IDE, building the project and download the program to the target board. More information about how to compile and program the project can refer to the
[Getting Started with MCUXpresso SDK](../../../../docs/Getting Started with MCUXpresso SDK.pdf).
Launch the debugger in your IDE to begin running the demo.
Expected Result#
When the demo runs successfully, you will find the LED is blinking.