Hardware requirements

  • Micro USB cable

  • MC56F80000-EVK board

  • Personal Computer

Board hardware common setting

  1. Power setting:

    Connect J8 pin2 and pin3 Connect J6 pin1 and pin2 Connect J5 pin1 and pin2

  2. Reset pin setting:

    Connect J11 pin2 and pin3

  3. Debugger setting:

    Connect J13 pin 1-2, 3-4, 5-6, 7-8

Board settings

No special settings are required.

Prepare the Demo

  1. Connect USB cable between the host PC and the J12 USB port on the target board. It setups Multilink and COM port in PC device manager.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board with Multilink debug configuration.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:

Starting PIT timer ...
 PIT timer interrupt is occurred !
 PIT timer interrupt is occurred !
 PIT timer interrupt is occurred !
 PIT timer interrupt is occurred !
 PIT timer interrupt is occurred !
 PIT timer interrupt is occurred !
 PIT timer interrupt is occurred !
 PIT timer interrupt is occurred !
 PIT timer interrupt is occurred !
 PIT timer interrupt is occurred !
...
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~