MCUXpresso SDK Documentation

Hardware requirements#

  • Mini/micro USB cable

  • MC56F83000 EVK board

  • Personal Computer

  • FreeMASTER 2.5 or later installed on PC

Board settings#

No special settings are required.

Prepare the Demo#

  1. Connect a USB cable between the host PC and the Debug USB port (JM60 USB) on the target board. Alternatively, use the USB-to-Serial interface at Boot USB port - see main.c for configuration option.

  2. Compile and download the program to the target board.

Running the demo#

  1. Run FreeMASTER and use connection wizard to connect at 115200 bps.

  2. Click on “FreeMASTER Demonstration Project (embedded in device)” on the Welcome page.

  3. Read more information about FreeMASTER tool at http://www.nxp.com/freemaster.